Eaton Logo

Anti-microbial

What is CuVerro?

Can CuVerro kill Ebola?

What does the EPA registration mean?

Is CuVerro® a surface coating?

What about silver?

Don’t copper alloys tarnish? What about tarnishing?

What are the public health claims being permitted by the EPA?

How is Antimicrobial Copper superior to other antimicrobial surfaces?

How does antimicrobial copper work?

What does the term “antimicrobial” mean?

Can CuVerro® antimicrobial alloys be used in food service applications?

How do CuVerro® surfaces compare to other antimicrobial surfaces?

Can CuVerro® surfaces be coated or waxed?

Do CuVerro® antimicrobial copper surfaces need to be cleaned?

How can CuVerro antimicrobial copper be used to kill bacteria* that cause infections?

What is the active ingredient in CuVerro® antimicrobial surfaces?

How quickly does CuVerro antimicrobial copper kill Methicillin-resistant Staphylococcus aureus (MRSA)?

Which bacteria (pathogens) has CuVerro® been proven to kill?

What is CuVerro Antimicrobial Copper?

Do you have to clean the CuVerro to maximize the killing properties of the copper?

What other applications could CuVerro be used in besides Healthcare?

Did you ever try Silver as an antimicrobial coating?

Do the switches have copper on them or is it a coating?

How Does CuVerro kill Bacteria?