Eaton Logo

What are the public health claims being permitted by the EPA?

Based on laboratory testing conducted under EPA protocols, when cleaned regularly, CuVerro surfaces:

  • Continuously reduces bacterial* contamination, achieving 99.9% reduction within two hours of exposure.
  • Kills greater than 99.9% of Gram-negative and Gram-positive bacteria* within two hours of exposure.
  • Delivers continuous and ongoing antibacterial* action, remaining effective in killing greater than 99.9% of bacteria* within two hours.
  • Kills greater than 99.9% of bacteria* within two hours, and continues to kill more than 99% of bacteria* even after repeated contamination.
  • Helps inhibit the buildup and growth of bacteria* within two hours of exposure between routine cleaning and sanitizing steps.