Eaton Logo

Aspire Z-Wave

Where can I find installation instructions for the Anyplace Switch?

How do I adjust the delayed time OFF on RF dimmer RF9540-N?

What is the minimum load for RF9540-N?

Can non-Eaton Z-Wave devices be installed with an Aspire RF system?

I have you RF9575 anyplace switch. Can I use it in an existing network?

If I need to replace a device, do I need to re-program all my scenes and events that included that device?

What is the maximum number of devices that can be associated to 1 Aspire RF switch/dimmer?

How many devices (nodes) can be included in 1 Z-Wave network?

What does a flashing RF device mean?

Can I monitor and control wireless Z-Wave devices from a mobile device or tablet?

Does the 5 button scene controller keypad control any loads?

Which half of an Aspire RF receptacle is controlled?

Do I need the Aspire handheld controller (or any other specialized controller) to program their scene controller (RFWC5 DW), or can I just program it through my Z-wave hub?

Do I need a separate controller to install RF9575 anyplace switch?

Where is the Install Button on an Aspire RF dimmer?

Where is the Install Button an an Aspire RF switch or accessory switch?

How many hops can a Z-wave signal make?

What is the difference between primary and a secondary controller?

Do all RF devices repeat the RF signal?

What is the maximum stated transmission range of a Z-Wave device?

Where can I find the User Manual for the handheld/tabletop controller (RFHDCSG/RFTDCSG)?

Does a lighted toggle switch glow when the switch is in the "ON" position?

What is the maximum amount of associations you can have in a RF system?

Is there such a thing as a 3-way RF switch?

Can I access wireless Z-Wave devices when away from home?

What does the "P" stand for on the hand held controller

I programmed scenes into your 5 button scene controller using Handheld. Do I need to keep handheld controller in the house for it to work?

What is the range of an anyplace switch?

Do you carry Anyplace switches?

How does how the anyplace switch work to operate a light fixture?

Is the controlled port of RF receptacle RFTR9505 capable of diming light?

What are types of “Child Lockouts” you can set up in an RF System?

Do Aspire RF dimmers need to be derated?

What is "Child Protection" in Aspire RF?

Where is the Install Button on an Aspire RF receptacle?

Where is the install button on an Aspire RF scene controller?

What is the amperage rating of Aspire RF receptacles?

What is the minimum load for RF9534?

What is the amperage rating of Aspire RF switches?

How can I change the ramp rate in an Aspire RF dimmer?

How many Aspire RF devices can be included in one scene?

What are the load ratings of RF dimmers?

My controller does not support association. How do I set up 3-ways and 4-ways?

What is association?

Can a secondary controller become a primary controller?

How many secondary controllers can 1 Z-Wave network have?

How many primary controllers can 1 Z-Wave network have?

How many scenes and events can be created using the Aspire RF handheld/tabletop controller?

What is an event?

What is a scene?

What is the frequency of the Z-Wave signal?

What prevents 2 different Z-Wave networks from interfering with each other?

What Aspire products do you offer?

Where can I find the drivers for the RFUSB-PRO?

If I don’t want to access my home network from outside the house, do I need a RFBER or RFTCP?

What is the longest ramp time (meaning slowest ramp rate) that can be configured for an Aspire RF dimmer?

What is a z-wave switch?

What is an any place switch?

What is the Derating for multi-ganged 1000 dimmers in an RF system?

How many devices can be included in one Aspire RF network?