Eaton Logo

Are the disconnect switches suitable for motor disconnect?

There is a difference between a motor controller and a motor disconnect. Both can turn the motor ON and OFF, but the motor disconnect has additional short-circuit current ratings and is considered more robust. The following are suitable for use as a motor disconnect: the AHDS-series, the X-Switch (30 and 40A only), ER4P-series fusible disconnects.