Eaton Logo

What would the IP rating be on two pin and sleeve mated with different IP rating?

The lower IP rating would be the rating of the connection. For example, if you mate AH430P5W  which is IP69 to the competitors 430C5W rated at IP67. the union would be rated at IP67.