Eaton Logo

Switches

What is the difference between a single pole and a 3-way switch?

Where can I find installation instructions for the Anyplace Switch?

What is the difference between a toggle and decora switch?

Where can I find installation instructions for LED Nightlight & Single Pole Switch?

What is a maintained contact switch?

Can I use 7501W or 1107W in older aluminum homes?

What is a rocker switch?

What Aspire line devices would be best for my house?

Do you offer a combination switch and receptacle that has a small indicator light on the switch?

Why do the decorator switches show a grounding screw when there is no screw on the ones i bought?

Do you carry a double pole, pilot light switch?

Do you have a switch with a timer?

What are the 7500 series switches made of

How does how the anyplace switch work to operate a light fixture?

Do you have gray switches?

Do you offer any switches with built-in timers?

Do you have a decorator switch for aluminum wiring?

What Co/Alr items do you have?

What type of fans do the fully variable fan controls work with?

What is the range of an anyplace switch?

Do you carry Anyplace switches?

Where can I find a non-preset toggle dimmer?

Do you offer auto ground feature on your switches?

What does CO/ALR stand for?

What is the difference between 7501 and 7501-9?